In a typical construction machine, lubricants amount to 2-3% of running costs. But 56% of premature bearing failures are caused by contamination and inadequate lubrication practices.
That’s why we talk not only about lubrication but also about lubrication lifetime solutions as an essential part of machine operation and vehicle maintenance.
We can never avoid failures of components exposed to friction, but with combined data insights and means of intervention, we can safeguard effectiveness and reliability, supporting asset health and sustainability. Using technology to improve the way we use our resources responsibly.
This is the next step in machine care.
The right
lubricant..
in the right
amount..
with the right
method...
at the right
time...
to the right
lubrication point...
Up to 33% lubricant savings by switching to automatic lubrication
How SKF Optimizes Your Equipment Performance
Save 20 Minutes Per Cycle by Automating Your Lubrication
Stay competitive by maximizing machine uptime with a holistic approach to lubrication:
Reduce Wear: Ensure precise lubrication at every point.
Avoid Downtime: Eliminate unplanned and unnecessary stops.
Save Time: Automate to save 15–20 minutes per maintenance cycle.
Beyond the 50%: Eliminate Premature Bearing Failure
Stay competitive by tackling the leading cause of downtime:
The Risk: Improper lubrication and contamination cause 50% of bearing failures.
The Solution: Automatic systems provide the right grease at the right time.
The Result: Longer maintenance intervals and maximum machine reliability.
Digital Control: Full Visibility, Less Risk
Bridge the skills gap while enhancing safety:
Automated Precision: Reduce the need for manual intervention.
Enhanced Safety: Lower the risk of maintenance-related accidents.
Digital Control: Monitor your entire fleet’s status via the SKF eLube app.
Still Have Questions?
See how we delivered results for the Volvo L150H in the case study below,
or get in touch today to start your journey toward 100% reliability.
CASE STUDY
Success Stories: Maximizing Uptime for Volvo
When a major construction firm in Singapore needed an urgent lubrication solution for their new Volvo L150H wheel loader, SKF delivered. Discover how we installed a custom SKF Lincoln automatic system under a tight deadline, eliminating downtime and ensuring precision grease delivery to 26 critical points.
View our lubrication brochures
Lubrication solutions for
construction machines
Where construction strength
meets SKF precision
SKF lubrication lifetime
solutions
Why SKF?
100+
Years of Innovation
71
Remanufacturing sites
15
Technology Centres
130
Countries
With over a century of engineering expertise, SKF transforms lubrication from a manual chore into a strategic advantage. We don't just provide grease and pumps; we deliver integrated, data-driven systems tailored to the harshest construction environments. By combining robust hardware like the Lincoln S203 with digital tools like the SKF eLube app, we help you eliminate the leading cause of bearing failure while simultaneously solving labor shortages and safety concerns. Choosing SKF means choosing a partner dedicated to maximizing your uptime, reducing your environmental footprint, and ensuring your fleet stays competitive on every job site.